MOTOR.IPEAK

General Information

Type

NV Parameter

Description

Sets the motor peak currentThe effective value of the peak current.

Units

mA

Range

0.200 to 1,000 A

Default Value

2.000 A

Data Type

Float

See Also

IL"Instruction list" This is a low-level language and resembles assembly.LIMITP, IL.LIMITN

Start Version

M_01-00-00-000

Description

This parameter configures the drive for the motor's peak, instantaneous-rated current. MOTOR.IPEAK is used to limit clamp the magnitude of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing q-component current command (IL.CMD ).

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™